Other Parts Discussed in Thread: PGA870, BUF634, OPA656, THS770006, THS4509, THS4520, THS4521, DRV1101, THS6204
A response to another of my questions on this forum, resulted in the TI moderator drawing my attention to the PGA870 Fully Differential Programmable Amplifier - which I wasn't aware of. It is possibly a better solution than what I had in mind.
My application is very similar to an oscilloscope - whose functional blocks can be used as an example.
Between the Oscilloscope's "input attenuator" and the pre-ADC "differential gain stage" is an "Impedance Converter" (Source Follower), which is a single-ended, high-impedance input to low-impedance, low-drift differential output block. As the input attenuator network typically has 1M impedance, the Impedance Converter must have a very high input impedance. Discrete solutions often incorporate a high-speed and low-speed path. Another objective is to have low DC drift.
Using a FDA to convert single-ended to differential-ended has too low an input impedance.
I was interested to discover that TI has the BUF634 high speed buffer which is single-ended input to single-ended output. Might TI have a single-ended input to differential-ended output part that is specifically designed for that Impedance Converter function?
I'm also interested in a similar part oriented towards slower frequencies as well (say 10kHz).
Thanks
Peter