Other Parts Discussed in Thread: OPA2604, ISO124, INA128, INA111
Hello Everyone!
Im currently working on my university final year project. My project is about constructing two similar EMG circuits (but differing in gain) to measure EMG from two forearm muscles called the Flexor Digitorum Superficialis (FDS) and Extensor Carpi Radialis Longus (ECRL). The outputs from the EMG circuits will be connected directly to a National Instruments SCC-68 Connector block with a PCI-6221 DAQ and computer running Labview 8.6 software. The purpose of this project is to find the relationship between the EMG signals measured from the forearm muscles to hand grip strength (measured using a hand dynamometer sensor). Experimental measurements from the EMG are to be taken while im gripping a hand dynamometer.
I have included an image of the EMG waveform from the circuit I have constructed to measure EMG from the Flexor Digitorum Superficialis muscle below. I have also included the circuit schematic I have used together with results from a short experiment I conducted to find the relationship between EMG frequency and hand grip strength. 6180.EMG_circuit.pdf
I used the INA128P instrumentation amplifer and OPA2604 operational amplifier for the band pass filters filters and additional stages. I used the driven right leg circuit to reduce common mode noise. Each of these circuits are powered by two energizer 9V batteries to supply +9V and -9V to each IC, therefore a total of four 9V batteries are used to power both the EMG circuits.
Since Im planning to connect the output of these EMG circuits to a National Instruments SCC-68 Connector block with a PCI-6221 DAQ and computer running Labview 8.6 software (which is powered by the wall socket power supply), what components should I include/add to this circuit in order to protect the subject? I have come across safety measures such as using the ISO124 isolation amplifier and optocouplers such as the HCNR200/201. This is a university class project and its not meant for medical or commercial purposes. I am working under the supervision of my lecturer.