Part Number: OPA2673
All,
I have seen SBOA120 and was wonder if there is a similar app note using capacitive coupling; I am coupling a low data rate signal onto AC line for PLC.
Thanks,
Regards,
Joe
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA2673
All,
I have seen SBOA120 and was wonder if there is a similar app note using capacitive coupling; I am coupling a low data rate signal onto AC line for PLC.
Thanks,
Regards,
Joe
Hello Joe,
Can you clarify? The App note you referred to includes AC coupling caps at both the inputs & outputs of the circuit (see figure 9).
Best,
Hasan Babiker
Hi Hasan,
Yes, there are capacitors on the input/ output however the coupling to the AC line is inductive, so I assume there would be some modification to the circuit if the coupling to the AC line were capacitive, maybe not.
Also wondering if capacitive coupling had been tried before.
Thanks,
Regards,
Joe
Hi Joe,
the transformer is really essential for the mains voltage coupling. It should not be omitted:
Kai
Hi All,
While the transformer is essential for mains voltage coupling (120/220VAC) what about low voltage AC? (~24VAC)
Or more broadly speaking: Is there a way to accomplish signal coupling while avoiding the use of a transformer? (Hence the capacitive coupling question)
Chris
Hello Chris,
The design wouldn't much modification to the circuit in the use case you are describing here. The main concern here would be ensuring you have proper filtering so that the AC voltage doesn't reach the outputs of the amplifier.
Best,
Hasan Babiker