Hello,
I'm using the pspice model of TLV6001-Q1 in SIMetrix 8.3, but there will run error when simulate, so is the pspice model cannot use in SIMetrix or need to edit the model?
If I edit the model, will it change the model performance?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm using the pspice model of TLV6001-Q1 in SIMetrix 8.3, but there will run error when simulate, so is the pspice model cannot use in SIMetrix or need to edit the model?
If I edit the model, will it change the model performance?
Thanks
Hello,
Did you use this method to import? 
Additionally, if importing the way shown above does not bring you success, I suggest to use our free simulation programs: PSpice for TI or TINA-TI.
All the best,
Carolina