Other Parts Discussed in Thread: INA193, INA240
When testing a very small current, how about the accuracy of the INA293?
As I know, when Vsense < 20mV, the acurracy of the INA193 will be very bad.
And I need to achieve a good control of a buck converter when the load is very light.
full load: 40A ,
light load: 1A ,
Rsense: 2mOhm,
Vsense: 80mV~2mV,
Peak current control
So I want to know the performance of the INA293 when Vsense is very small.
Or there are some other chips better than INA293.