Part Number: OPA2333
1. The following circuit of opa2333 is shown in the figure. Is R7 required? Why?Are other operational amplifiers needed?
2. Can internal clamping diodes be used? In case of over-voltage, the clamping diode current is 0.7ma, less than 1mA in the manual. Is it OK?
3.Does the output of the op amp need a resistor in parallel to ground to ensure that the op amp has some load? If R12 in the figure is needed, how big is the resistor?