Other Parts Discussed in Thread: TPS2373, TPS2372, TPS23755, TPS23758
Hi,
As per our new requirement, we have to design the 2 port wired router with PoE. the Device has 2 port POE with capable of 1000 base t data transfer. One end act as PoE PD and receives the power up to 30W (IEEE 802.3at, Class 4) from the main PoE source, on the other end act as a PoE PSE which is re-transmit the 15W or lesser (IEEE 802.3af class 3/2/1) power from the received power. Please confirm the possibility of the above power conversion. If it Is possible, please guide me on the concept.