This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Pole cancellation: how to?

Hi to all users.
I have following question for experts:

here my analog system model as an high pass filter (first block)

poles at 0.16 and 106 Hz.

second block is a bandpass filter at 0.5 Hz, so final transfer function is:

This is a band-pass filter (0.5Hz to 106Hz).
I need flat response over 0.5Hz, so I need to remove pole at -666.67.
My first idea was to use inverting amplifier OP AMP with capacitor in parallel to resistor....
Any suggestion?
Thanks.