Other Parts Discussed in Thread: OPA196
Hi to all users.
I have following question for experts:
here my analog system model as an high pass filter (first block)
s^2/(s^2+667.67s+666.67)=S^2/[(s+1)(s+666.67)]
poles at 0.16 and 106 Hz.
second block is a bandpass filter at 0.5 Hz:
s/(s^2+6.06s+9.18)
so final transfer function is:
s^3/[(s+1)(s+666.67)(s^2+6.06s+9.18)]
(sorry, image and formulas copy doesn't work)
This is a band-pass filter (0.5Hz to 106Hz).
I need flat response over 0.5Hz, so I need to remove pole at -666.67.
My first idea was to use inverting amplifier OP AMP with capacitor in parallel to resistor....
Any suggestion?
Thanks.