Other Parts Discussed in Thread: PSPICE-FOR-TI, , LMP2231
My customer said: In a PSPICE-FOR-TI there is model, but it can it cannot be put on the schematic.
Can you please check what could be an issue.
Thanks
Viktorija
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My customer said: In a PSPICE-FOR-TI there is model, but it can it cannot be put on the schematic.
Can you please check what could be an issue.
Thanks
Viktorija
Per customer:
Some parts in PSPICE have Open Reference Design and simulation model. If you try for example LMP2231, click on it, when is highlighted right mouse click, you will see it on the menu.
The most interesting parts for me do not have this option. This is very useful for choosing components.
Thanks
Viktorija
Viktorija,
We do have a collection of test circuits that you may place LM2904 into, along with instructions on how to use each test circuit in this app note. This app note contains a link to a PSPICE and TINA-TI repository of test circuits. I've linked the app note and the test circuits here, and you can forward these to the customer as well.
While this isn't pre-set up to match supplies and load conditions from the datasheet of LM2904, these circuits allow for you to enter and test the conditions you would like to use in your application.
Hope this helps,
Jerry