Part Number: INA826
Experiencing temperature related output drift in unity gain operation. If the circuit board heats up or I introduce a small amount of heat to the chip, say 10°C, I see 50 - 100mV change in the output. I've even replicated this circuit with the INA826 Eval board without the sensor attached and substituted for a power supply with the same result. Any help is greatly appreciated!
**EDIT**: Refer to the schematic in the post below: My reference input is: SNGL_VREF_IN = 2.5V and Sensor Output is: SNGL_I_IN = 2.5V. **/EDIT**