Part Number: TL331B
Other Parts Discussed in Thread: TL331, LM393
We test the TL331B has a problem below,
1. After remove the DC power, during the VCC(VZ) voltage drop to 4.25V, the output (PIN 4) has a high-frequency jump, which is not our expected phenomenon
2. The datasheet indicates the working voltage 3V-36V, the 4.25V should be considered as normal working conditions, and there should be no jitter
3. The same PCB, only replace new TL331, the output will be work normal.
Do you have any recommend? Thanks
BR,
Gary