This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XTR111: Minimum load resistance

Part Number: XTR111

Hi, 

Good day. I hope you are doing fine. 

Our customer wants to know the minimum load resistance that they can use. 

I hope you could help us on this matter. 

Thanks. 


Regards,

Cedrick

  • Hi Cedrick,

    Our customer wants to know the minimum load resistance that they can use. 

    XTR111 is a voltage to current converter or transmitter. Since the output is a constant current source, the load resistance is dependent on the constant source currrent and XTR111's supply voltage. 

    For instance, it the circuit is supplying 20mA and max. supply voltage is 24V, then the max. load resistance is approx 24/20mA or 1200 Ohms. Or with 1 kohm resistor as load, the voltage across the resistor will be 20mA*1kohm = 20V. 

    Regarding to the minimum load requirements: 

    Because the output is constant current source, you may short the output load, if you have to, except you need to make sure that there are no heat dissipation issues at Q1 and 15 ohm etc.. If you short at the Rload in the schematic below, if Iout = 20mA, then the voltage across the 15 ohm resistor is 0.3V, Assume Q1 has  Rdson around 0.1Ohm, its heat dissipation will be 20mA*20mA*0.1ohm = 40 uW, which Q1 will be happy. 

    If you have other questions, please let us know. 

    Best,

    Raymond

  • Hi Cedrick,

    because the output signal of XTR111 is driven by a current source, there's no minimum load resistance. The customer can decrease the load resistance down to 0R, if he wants :-)

    Kai