Part Number: INA260
Is there an impact on current sensing connecting the VBUS pin to IN- instead of IN+ ?
Thx & regards
MW
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi MW,
For all practical purposes, there is no difference connecting to IN- versus connecting to IN+.
Connecting to IN- excludes the shunt voltage from the Bus voltage measurements, and the resulting Bus voltage is the actual voltage dropped across the load. As a result measured power is closer to the power actually delivered to the load.
Given that shunt voltage is much smaller than Bus voltage in most applications, connecting to IN- or IN+ makes little difference.
There are other minor differences of even less importance, they can be ignored. You have the freedom to connect to either.
Regards, Guang