Part Number: INA332
Other Parts Discussed in Thread: INA818
I am considering using the INA332 to amplify a 60 kHz sine wave. The INA332 will drive other op amps to increase the output level to 5 volts.
I have questions about the circuit I have attached. Can the two 10k resistors (R1 and R2) be eliminated? A 1.1 mH inductor will be connected across PL1 and will resonate at 60 kHz with C1, C2, and C3. C3 is currently shown as TBD but is approximately 150 pF.
The input signal will vary between 50 uV and 4 mV. Do I have the biasing correct to allow this input range to work?
Thank you.