Part Number: OPA2180
Hi Team,
Please help recommend suitable isolated resistor(R79) and feedback resistor(R47) value regarding to below customer's application. Many thanks.
Best Regards,
Stanley.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA2180
Hi Team,
Please help recommend suitable isolated resistor(R79) and feedback resistor(R47) value regarding to below customer's application. Many thanks.
Best Regards,
Stanley.
Hey Stanley, putting that R79 inside the loop is a bad idea, just creating another loop pole - putting it outside the loop works a lot better where then R47 can be zero ohm.
The load C looks like 1uF ?
Maybe an R79 outside the feedback loop of 20ohm would be adequate for good phase margin without excessive bandlimiting to the load C.
Hi Stanley,
Here is a loop stability plot Michael suggested:
If the Vref's resistitive load is high, then you will have tighter 1.5Vref. You may have to adjust R4 value accordingly, somewhere around 500Ohm range with 1uf capacitive load. As it is presented, you have approx. 78.8 degree of phase margin. Enclosed is the simulation.
/cfs-file/__key/communityserver-discussions-components-files/14/OPA188-HZ-10192020.TSC
If you have additional questions, please let us know.
Best,
Raymond
Hi Stanley,
Q: Can you please recommend suitable RF and CF value here?
With the following configuration, your BW of the circuit is approx 1.25kHz. If you are using the 1.5V as voltage reference, may be it is adequate.
With 1khom load, you will have approx 64 degree of phase margin, see the simulation. If R5 is reduced to 200-300 ohm range, you may increase the loop-gain slightly, but your phase margin will be reduced.
/cfs-file/__key/communityserver-discussions-components-files/14/OPA188-HZ-10202020.TSC
Best,
Raymond