Part Number: LM2901
Team,
My customer has the following question:
Can you tell us why LM2901M (-40°C to 85°C) and LM2901D (-40°C to 125°C) have different specified operating temperatures when Reliability and MTBF tests for LM2901M are conducted at 125°C? Also, the power rating on the datasheet for LM2901M discusses derating at a junction temperature at 125°C. Should LM2901M not be operating at temperatures above 85°C?
Regards,
Aaron