This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM311: input impedance

Part Number: LM311

Hi Team,

Customer wants to know what is inverting node common mode impedance?

Cannot find this info in datasheet, thx!

Andrew

  • Hi Andrew,

    For DC signals, the input resistance can be approximated to Vcm/Ib. Note that the 3pF input capacitance is in parallel to this DC resistance. So as the frequency of the input signal increases, then the reactance of the capacitor (Xc) dominates the resistance seen at the input.

    In shorter terms, low frequency means input resistance is approximately Vcm/Ib. As frequency increases, the input impedance is dominated by the 3pF input cap.

    I hope this helps.

    Regards,

    Joe