Part Number: INA111
Other Parts Discussed in Thread: OPA192
Hi,
We are considering using this device.
While checking the graph information, I found a peculiar characteristic.
Could you tell me about Gain vs Frequency graph?
1.
The amplification factor increases in the range of 1MHz to 2MHz under the condition of "Gain = 1".
Is this phenomenon unique to INA111?
Could you tell me the reason why the amplification factor increases at the point of "⓵"?
And Does this increase phenomenon depend on individual differences and temperature?
2.
Under the condition of "Gain ≥ 10", the amplification factor increase phenomenon does not occur.
Is there any reason why the increase phenomenon does not occur at the "②" point?
Is it possible that it will occur due to temperature or individual differences?
Best regards,
Yusuke