Part Number: LM258
hi team:
1. Please help to review the schematic
2. The power supply voltage input is 24 V, and the signal voltage input is 0-3.3 v
3. The defective products are sent to the terminal customers after the normal trial production (including function test) in the customer's factory, with a total of 20 PCs. the feedback of such defective products is 1pcs, and the defect rate is 1 / 20;
Normal IC: Pin1 impedance to ground is infinite;
Abnormal IC: Pin1 impedance to ground is about 10M Ω;