Part Number: AMC1100
Other Parts Discussed in Thread: TIDA-00555, AMC1311
I am planning to use the AMC1100 on a new design and I am having problems understanding the common-mode operating range of the device.
I would like to sense an AC voltage in a circuit configuration such as in TIDA-00555, whith an isolated power supply for the AMC1100.
- On the one hand, in the datasheet it is stated that the common-mode operating range shall not go under -0.16V.
- On the other hand, in such a AC application, if I connect GND1 to VINN and use the full ±250mV differential input voltage range, my common-mode voltage on VINP would go down to -0.25V, which violates the previous operating range.
Since the "absolute maximum rating" for analog input voltage is GND1-0.5V I think the device will not collapse, but I would like to know how all these parameters play together.
Should I constrain my AC sensing to an input range of ±160mV? Or did I understand something wrong?
Thank you in advance!