Part Number: INA105
Other Parts Discussed in Thread: TINA-TI
Dear Support,
in my application, I need to sink/source a (very)-low-noise current (range: 100nA -> 100uA) into a low impedance load (about 50 ohm) to ground.
The current noise should not exceed the thermal noise of a few MOhm resistor (in the range from 1M to 10M).
I am considering a Howland current generator designed around the INA105. The circuit is taken from the app note:
-> please, see fig 51 at page 21.
The TINA-TI schematic is attached here:
With this circuit, in order to have 100uA with a 10V input, I have to select a 100k resistor.
Unfortunately, the output current noise is dominated by the thermal current noise of such a 100k resistor (4 x 10^-13 A/sqrt(Hz)) , so I am very far from the noise level I am looking for (5 x 10^-14 A/sqrt(Hz) at the most).
Am I doing something wrong ?
Could you please suggest me a solution, based on Howland scheme or on any other circuit capable to fulfill my requirements in terms of current range and noise.
Thank you in advance for your time and support,
Alberto