This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS7530-Q1: Gain control signal and external resistor network for adjustable gain

Part Number: THS7530-Q1
Other Parts Discussed in Thread: THS7530,

Hi team, 

Could you tell me what "gain control bandwidth" mean? 
I guess "gain control bandwidth" is just for an input signal for VG- and VG+ which is separate from "small signal bandwidth", is it correct?

In addition, can we make its gain range to 5dB to 15dB from 11.6 dB to 46.5 dB (datasheet gain setting spec) by configuring external resistor network?

Regards,
Ochi

  • Hi Yoshiki,

    assume the gain control bandwidth is 1kHz and you give a sine of 100Hz to the gain control input. Then the amplitude of output signal will change hundred times per second with full change of amplitude, exactly like AM modulation. But if you give a sine of 100kHz to the gain control input, the amplitide of output signal will not show any change of amplitude because the modulation signal is way beyond the gain control bandwidth then.

    Translated to the THS7530 the gain control signal can have a frequency of up to 15MHz.

    Kai

  • Hello Ochi-san,

    Yes the gain control bandwidth is just as you mentioned and Kai has explained. The gain range is internal to the amplifier and isn't set by external resistors.

    Best,

    Hasan Babiker 

  • Hi Kai-san and Hasan-san, 

    Thank you for making clear understanding THS7530-Q1 gain control feature.

    Regards,
    Ochi