Other Parts Discussed in Thread: ISO120
Hi,
The ISO120 has an application note to boost the BW of the device to 100kHz (which is what I need). I plan to use the ISO amp to separate an amplified signal from an amplifier stage (between 1-5V) and the oscilloscope to break the ground loop. So I guess the current requirements are not so high since I'm basically doing a voltage reading at 100kHz bandwidth.
1) However, I want to pick passive components that will contribute small noise and handle the power requirements of that circuit. Do you have suggestions on the type of power I need for the passive components and the type of passive components that I will need? (ie. film vs. carbon resistors, capacitor types, etc).
2) On another note, the power requirements show +-15V supplies. But, I want to run this amplifier circuit using batteries and preferably with only 1 supply. Is this possible? What do you recommend for the power? Would I require any regulation or can I use a simple passive regulation of the battery power?
Thanks!