Other Parts Discussed in Thread: OPA2388, OPA376, OPA333, INA826, OPA320, INA821, OPA2380, OPA145, OPA1612
Hi everyone,
I'm developing an ECG test-bed for analog output front-ends as an academic project. The ECG signal is generated by a DAC and is attenuated with a resistive devider, at its output it presents a very low amplitude (on the orders of 100 uV to 5 mV). The divider's output must be buffered before entering the ECG front-end. To avoid a major decrease in SNR, this application requires opamps with very low noise figure (under 1 uVpp).
The ECG signal is mainly composed of very low frequency harmonics (from 0.5 Hz to 30 Hz). For the lowest possible noise figure (between 0.5 and 30 Hz) it seems that the OPA388 is the ideal operational amplifier.
The questions that I'm asking are:
The OPA388 is really 1/f noise free? In the datasheet there are no traces of flicker noise back to 1 Hz, does it occur at lower frequencies or does not occur at all?
Are there other operational amplifier options from TI which offer better noise figures, for this bandwidth (0.5-30 Hz)? While being RRIO or wide common-mode voltage input range for single supply operations.
Which are the models currently offered by TI which have no flicker noise (or very low figures) ?
I'm sorry for making all these questions, but it is difficult to find low flicker noise operational amplifiers, since there are no search filters for input voltage noise (between 0.1 Hz and 10 Hz), or low flicker noise, only input voltage noise density (at f = 1 kHz).
Kind regards,
Daniel Almeida