Part Number: THS3217
Other Parts Discussed in Thread: THS3215
Hi Team,
We have designed a DAC circuit with using THS3217 part. Our design requirement as below,
- Bandwidth (-3dB) at least 10MHz
- Support output range +-5V
- Output drive current >=25mA
- Flatness> less than 0.5dB
But as per the below simulation model, we have getting very large -3db gain/frequency bandwidth (836Mhz) and also Bandwidth Flatness is more than 2dB.
Could you please suggest how to adjust output -3db bandwidth and improve the bandwidth flatness.