Hello team,
I need to identify replacement op amps for the MC33071, MIC6211, and NCS20071 devices. What are the best P2P (Pin to Pin) replacement amplifiers from TI?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
I need to identify replacement op amps for the MC33071, MIC6211, and NCS20071 devices. What are the best P2P (Pin to Pin) replacement amplifiers from TI?
Thanks!
Hi Kiernan,
You can look at our newest high voltage op amp, TLV9351, which is a 3.5MHz, single-channel, 40V and low noise amplifier. It’s cost-optimized and the slew rate is as high as 21V/us.
Here is a table showing the performance differences between MC33071, MIC6211, NCS20071, and the recommended device:
Thank you,
Tim Claycomb