Part Number: OPA462
Hi Team,
A customer supplies 170-180V to OPA462 and the device turns hot. Whenever he reduced the supply voltage the device cools down. Upon checking the quiescent current of the device, it consumes 2mA which translate to 180V x 2mA = 0.36 watts of heat. He did not connect the thermal pad to ground so there will be no thermal path from the device to the board except for the V- of the device.
Looking at the PCB layout at page 11 of the user's guide of OPA462EVM it seems that the thermal pad is not connected to ground as well. Can you please confirm?
Regards,
Danilo