Part Number: BUF634A
Other Parts Discussed in Thread: OPA1656, , BUF634, OPA2810
Working with this composite circuit shown in the OPA1656 PDS. If you parse through 5Vpp input at gain of 2 in the curves, that is +/-5V output into a min load of 16ohms. Which of course will require +/-5V/16ohm = 313mA (and a little more for the 1kohm load in the feedback path.
Pretty good THD, so apparently this works even with the typ continuous output current spec of +/-250mA. That is not unreasonable as the peak output current is always greater than continuous - however, this kind of undefined region can run into short circuit current non-linearity - that spec. shows typ and max, but perhaps the min number would be needed for these peak current designs exceeding the continuous?