Part Number: LM393
Hi,
Could you tell me the input impedance (IN+,IN-) value of LM343?
Customers need specific value information for connection and design with other circuits.
Regards,
Yusuke
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM393
Hi,
Could you tell me the input impedance (IN+,IN-) value of LM343?
Customers need specific value information for connection and design with other circuits.
Regards,
Yusuke
The inputs are the bases of PNP transistors and do not behave like resistors.
Section 2.1 of Application Design Guidelines for LM339, LM393, TL331 Family Comparators says:
All PNP emitters in the Darlington input stage have current source connections. These current sources ensure a consistent input bias current that does not vary with the differential input voltage. This consistent current provides a high effective input to input resistance.
Your customer's circuits must be able to sink the bias currents.
Hi Tsukui,
it can be estimated from the following figure of datasheet:
For a supply voltage of 5V and 25°C die temperature we get
Zin ~ delta U / delta I = (2.5V + 0.25V) / (2.75nA -2.25nA) = 5.5GOhm,
superimposed to a DC input bias current of -2.75nA at Uin = 0V. The "-" sign means that the static input bias current is flowing out of the device :-)
Kai