Hello Team,
My Customer is looking for the thermal information of TLC2252AM, can you share the data with us?
Regards,
_Renan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team,
My Customer is looking for the thermal information of TLC2252AM, can you share the data with us?
Regards,
_Renan
Hi Renan,
This is the thermal information in this part, if I understood your question correctly. Yes, the data is presented in different format. I believe that these figures refers to Junction to package thermal power dissipation.
For Instance in JG package. the nominal specific power rating is 1050mW (Ta <= 25C). Derating factor is 8.4mV/C above 25C.
For Ta=70C, the delta Ta = 70-25=45C, derating power dissipation in mW is rated 8.4mW/C*45=378mW --> power dissipation 1050mW-382.5m <= 672mW at 70C
For Ta=85C, the delta Ta = 60C, derating power dissipation in mW is rated 8.4mW/C*60C =504 mW --> power dissipation 1050mW-504m <= 546 mW at 85C
For Ta=125, the delta Ta = 100C, derating power dissipation in mW is rate 8.4mW/C*100C =840 mW --> power dissipation 1050mW-840m <= 210 mW (power dissipation is specified <275mW at Ta=125C)
If you are interested to see the derating factor in C/W figure, you can inverse 11.0mV/C to 90.1C/W (equivalent to Junction-to-case thermal resistance as an example).
If you have other questions, please let me know.
Best,
Raymond