This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS4541: About Vocm

Part Number: THS4541


I have a question about THS 4541 data sheet page 40.

In an AC-Coupled, Differential-Input to Differential-Output configuration,
When Vs + is connected to 5V and Vs − is connected to GND,
Is it correct that Vocm is set to 2.5 V ( defaults midsupply) when opened?