Part Number: LM7171
Other Parts Discussed in Thread: THS4012, THS4022, LM6172, OPA862
Hi Team,
A customer would like to design a single to differential stage using the LM7171 opamp. Since the LM7171 come in single channel package, how good is the propagation delay matching to be between two such opamps?
In his application he will have 20ns rise/fall times, so the propagation delays of the 2 opamps (5ns typical) should not vary drastically. He had looked for 2-channel opamps that would have very close matching, being in the same die, but the results were not as good as with LM7171 (for example LM6172 and THS4012/THS4022).
He don't mind about the exact number of the propagation delay, he just need them to be close for the two discrete opamps.
Regards,
Danilo