Part Number: OPA462
Hi,
Could you let me know E/D pin is left to open?
If not, please let me know proper connection.
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA462
Hi,
Could you let me know E/D pin is left to open?
If not, please let me know proper connection.
Thanks.
Hello David,
Section 7.3.4 in the OPA462 datasheet, "Enable and Disable" provides information for applying the E/D pin. It indicates that you can leave the E/D pin and the output will be enabled. But because the E/D pin is a very high impedance pin it suggests that a small capacitor such as 30 pF be added from the pin to ground. That helps keep the pin from changing state should a fast impulse on an adjacent trace be coupled to it. Section 7.3.4 and Figure 60 provide you with alternative connection information for the E/D pin.
Be sure you solder the PowerPAD, underneath the OPA462 package, to a PC board pad that is connected to the V- (-75 V) supply potential. The datasheet discusses the connection on Page 28, in Section 10.1.2, PowerPAD™ Integrated Circuit Package Layout Guidelines. That is sometimes overlooked and can result in unexpected issues.
Regards, Thomas
Precision Amplifiers Applications Engineering
Hi Thomas,
When E/D com is connected to -75V, what connection do you recommend?
30pF@E/D to GND or 30pF@E/D to -75V?
Thanks.
Hi David,
Section 7.3.4 states "a conservative approach is to connect E/D through a 30-pF capacitor to a low impedance source." The Figure 60 schematic shows the capacitor connected directly to ground. The V- supply should work as well because the supply bypass capacitors connected back to ground. However, for simplicity's sake I would connect it to ground.
Regards, Thomas
Precision Amplifiers Applications Engineering