Part Number: AMC1301
Hi Guys
AMC1301 is being used to sense AC input voltage. After filtering, Vac1_LINE and VAC1_NEUTRA are directly input to MCU, and AGND is connected to AC1_SGND. R159 and R160 are not soldered, and when C156 and C157 are 0.1uF, Vac1_LINE and VAC1_NEUTRA have large ripples. After removing C156 and C157, the ripple disappears. After replacing it with 4700pF, the ripple becomes smaller but still exists.
From the AMC1301 datasheet, it can be seen that the output of the isolated op amp has no capacitance to ground. Are these two grounding necessary? What is the reason for the ripple?
Test waveform:
1.Remove C156, C157, CH1: Vac1_LINE and VAC1_NEUTRA CH2: Resistance string sampling Vac
2. C156, C157 4700pF , CH1: Vac1_LINE and VAC1_NEUTRA CH2: Resistance string sampling Vac
3.C156, C157: 0.1uF CH1: Vac1_LINE and VAC1_NEUTRA CH2: Resistance string sampling Vac
Thanks
-Vincent