Hi Support team
VCCS1=11V
12V=12.3V
12VF=12.6V
shunt resistor = 0.1m ohm
max output current : 160A
0.1m*160*500= 8V
12VIO= 8V
base on following application circuit,
I have few questions
1. what is suitable value of input filter, C607, C610 and C611
2. what is max output current for this application? can INA211 support 160A output current
3. any side effect?
thanks a lot