Hello,
I have a requirement to convert a Digital 24-bit RGB +HVsync to RGB analog with separate digital HVsync signal. The display resolution is fixed at either 854x480 or 854x600 progressive scan at 60Hz. I believe this resolution lies between EDTV and HDTV.
The analog signal to the display must be 0V to 0.7V peak to peak with no offset for blanking or sync, as the sync will be driven separately by the THS8200.
I am considering using one of the THS731x family of devices with internal LPF but because of the display requirements not sure which device would be best suited. This device needs to be very small and low powered and powered from a single 3v3 power rail.
The displays will be located fairly close to the op amps about 4 inches, my preference would be to have DC coupling between the displays and the op amps.
Thanks,
Bob