Dear all,
I wish to receive a clarification of the paragraph on page 10 of the OPA847 datasheet which states:
"If the signal source is actually the low impedance output of
another amplifier, RG should be increased to be greater than
the minimum value allowed at the output for that amplifier
and RF adjusted to get the desired gain. It is critical for stable
operation of the OPA847 that this driving amplifier show a
very low output impedance through frequencies exceeding
the expected closed-loop bandwidth for the OPA847."
My circuit takes the output of a low-gain transimpedance stage based on the OPA847 and amplifies the voltage with a gain of -40V/V in a second inverting gain stage also using an OPA847. What exactly would be a large enough value of RG to place at the output of the first OPA847? I was thinking RG= 50R with a feedback of 2K in the inverting gain stage to give -40V/V. However, this has not proved to operate well in practice.
Thanks.