This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMC7101: Clarification on LMC7101BIM5/NOPB and applicable qualification test report for the updated part

Part Number: LMC7101


Hello,

Per PCN# 20201022000.1- Qualification of TI Philippines as an additional Assembly site for select devices

The material is being updated for Part Number LMC7101BIM5/NOPB, can you please confirm that the thermal, electrical, mechanical properties remain the same for the updated part.

Also, please share reliability/ qualification report for the updated part.

Regards

NEHA PANDEY

  • Hi Neha,

    I will look into the details of the PCN. I will get back to you as soon as possible.

    Thank you,

    Tim Claycomb

  • Hello Neha,

    PCN informational request can be made through the TI customer support center, here.

    Per PCN 20201022000 the addition of a second source Assembly Site for select devices, including the LMC7101BIM5/NOPB was completed and qualified. The current assembly sites and Material differences are noted in the PCN. At this time no update to electrical characteristics or electrical specification have been identified in the PCN or within the TI product datasheet.

    The qualification details are listed within the PCN itself under the section titled "Qualification Report". The Product qualification was completed per industry standard JEDEC for the selected devices.

    Regards,

    GPAMPs Quality

  • Thank you for the quick response. Please confirm which of the following qualification device/ QBS Package applicable for Part Number LMC7101BIM5/NOPB - 

  • Hi Neha,

    Can you please try to repost the image? You need to use the "insert media" icon to insert pictures in your reply.

    Thank you,

    Tim Claycomb

  • Hello Neha,

    All devices listed within the qualification report provided in the "Qualification Report" section of PCN 20201022000 are utilized for QBS. The LMC7101BIM5/NOPB was QBS'ed to the qualification devices listed.

    For additional questions regarding PCN's it is recommend to contact the customer service center. E2E is typically for application support.

    Regards,

    GPAMPs Quality

  • Thanks Tim, 

    I am referring to the snapshot from the PCN, it is showing 3 different qualification device and 3 different QBS package in the qualification report. Which one of these will be applicable for part LMC7101BIM5/NOPB

  • Hi Neha,

    I recommend following Joseph's instructions in the previous post to contact the customer support center. There you will be able to request additional PCN information.

    Thank you,

    Tim Claycomb