Part Number: INA282
Other Parts Discussed in Thread: INA210, INA302, INA240, INA190
Hello,
I am Using current INA282 Current sensor (Bi-Direction).
My Current range is from 100mA to 13.5A in one direction and in another direction the Current range is 100mA to 7.5A.
Voltage range is from 800mV to 70V on both the direction.
Supply voltage for the IC =5V
My ADC ref is 4.09V
I need to measure each 1mA current.
I am attaching my circuit and calculation.
Could you please let me know whether my circuit is ok or any better circuit can be used.