Part Number: LM7321
Other Parts Discussed in Thread: OPA2990, OPA2991
Hi Sirs,
May I know there have any devices can support the Vin differential range up to +/-12V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Henry,
You may want to look at the portfolio of fully differential amplifiers, which may be more useful in your search.
Best,
Jerry
Hi Henry,
What is the need for a differential voltage up to +/-12V? Are you intending to use the op amp as a comparator?
Our new high voltage op amps (40V) such as the OPA2990 and OPA2991 has an absolute maximum input differential voltage rating of Vs+0.2V.
Thank you,
Tim Claycomb
Hi Tim,
Thank you for your sharing.
My customer will using the op amp as a voltage buffer.
Hi Henry,
If the customer is using the op amp in a buffer configuration then they should not have to worry too much about the abs max differential input voltage limit. When it is in a buffer configuration the op amp is in a closed loop configuration and the op amp will drive the two inputs equal to each other.
The customer would need to worry if their input signal caused the output voltage to rail to one of the supplies and the input signal kept increasing. This condition would cause a differential voltage at the inputs because the output would no longer be able to regulate the inverting input equal to the non-inverting input. However, in a buffer configuration this is unlikely to occur and would require an input voltage greater than the supply voltage which would cause the internal ESD diodes to turn on.
Thank you,
Tim Claycomb