This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi sir,
I wanna select a current sense,
My circuit current is wide range from 10mA to 2A.
voltage is 1.1V 1.5V 2.5V and so on.
is INA216 meet my requirements?
If not, can you suggest a recommended product?
Thank you for your valuable suggestion.
Regards,
Frank,
Can you share what you mean by "voltage is 1.1V 1.5V 2.5V and so on." Are you saying that your maximum voltage that you can supply the amplifier with is a maximum 2.5V?
Based on the lower range of measurement in the mA range, as well as potentially the limited voltages above, I would recommend looking at the INA186 or INA190. These devices are capable of operating down to a 1.7V supply range, and have input bias currents in the picoamp range, which will help reduce error in the lower decades of your measurement.