Hi,
Previously I've made a circuit for uA - A range currents , which seems to work reasonably well (with calibration).
For high current range the circuit uses 40mOhms resistor with a PGA281 with 32x GAIN. For lower currents the setup is the same just with 10 Ohm.
I'm trying to make a switching circuit , which could switch automatically really fast between the two range with bypassing the 10R resistor with a low Rds FET.
The planned switch threshold would be around 4-8mA . I'm planning to control the switch based on voltage drop on the 40mOhm resistor. However this voltage is around 0.16-0.32mV. I'm afraid that a simple comparator wouldn't work with that low voltages. I'm trying to configure and simulate different opamps to amplify the signal before comparison, but I couldn't find one to perform this task according to my needs. Preferably below 1usec.
Could you please help selecting the right parts ?
Regards,
Gabor