Part Number: PGA309
Other Parts Discussed in Thread: XTR117, XTR111, , XTR115
BS"D
Hi,
We work with the TI IC PGA309 in many projects. Basically, in one project where we convert the voltage output from the PGA to a 04-20mA, 2 wires output current (using the XTR117).
In order to calibrate our Load cells with these circuits in production we use the MultiCal System also provided by TI.
Now we have another project where we need to use the PGA309+XTR111, that is also 04-20mA but only in one wire current output to ground. The fact is that I can calibrate with the PGA309EVM-USB but we need something more automated in production like MultiCal. The question is if it is possible to use the MultiCal System with these new project? Just in case, could you tell us how to connect all the wiring to calibrate our Load Cells accordingly?
I am looking forward to hearing from you soon.
If you need any detail, schematic or clarification don’t hesitate to tell me.
Kind regards