Part Number: THS4304DBVEVM
Other Parts Discussed in Thread: THS4304
Excuse me, is there a recommended circuit for THS4304 single power supply?
Are there any restrictions on single power supply?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: THS4304DBVEVM
Other Parts Discussed in Thread: THS4304
Excuse me, is there a recommended circuit for THS4304 single power supply?
Are there any restrictions on single power supply?
Hello 武奇,
The THS4304 is designed to be operated in a single supply while retaining functionality. All of the figures present in the datasheet present data from a single supply configuration of +5V or +3V, often with a gain of 2V/V. You may see the Application Information section on page 15 of the datasheet for more information on application and use cases.
Kai referenced an important figure (which you also found, Fig. 54). The text above Figure 54 also asserts how the single supply configuration can be configured with no performance loss compared to the +/- 5V dual supply.
Could you elaborate on how you intend to use the THS4304, as well as how the single supply configuration has not worked for you?
Best,
Alec Saebeler
Hello,Michael:
I am using THS4304 for differential to single-ended conversion. According to the documents you provided, can THS4304 that was powered by a single power supply use for differential to single-ended conversion?
Best Regards
Qi.Wu
Well Qi
The THS4304 is a very fast VFA device but is not RR output. In fact it requires about 1.1V headroom to each supply for correct operation, this means on 5V single supply, the output can only swing 1.1V to 3.9V. If your circuit and inputs try to go outside those limits it will clip and recover slowly