Is it possible to simply generate a 4-20mA current signal with XTR115U without wiring it in a 4-20mA loop? I have a project where the customer would like to design a single PCB that is capable of handling 2 wire sensors(+, mA) and 3 wire sensors (+,-,mA). Currently, I've have 2 wire mode working on my prototype board. In 2 wire mode the XTR115U has a separate reference from the 4-20 loop and the references are connected at single point through a 25 ohm resistor (first figure in the datasheet connects Iret to Iout through 25 ohm resistor). When in 3 wire mode, I would like to just feed Iin with a voltage and have the XTR115U generate a 4-20mA signal and output it through Iout. In my attempt for 3 wire mode I left Iret unconnected from the reference and connected Iout to the reference, but I'm only getting 2.97mA through Iout with a Iin voltage of 400mV. Am I missing something here in my attempt or is not possible for the XTR115U to genereate 4-20mA without being looped powered?