This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TINA-TI: MOSFET spice model import

Part Number: TINA-TI


Hi,

I'm trying to import DMP2003UPS spice model to TINA-TI via new macro wizard. I believe I'm making it right. However after importing, de FET doesn't seem to work as it should. In a complex system it gives a convergence error. 

Could you please check ? 

*---------- DMP2003UPS Spice Model ----------
.SUBCKT DMP2003UPS 10 20 30
* TERMINALS: D G S
M1 1 2 3 3 PMOS L = 1E-006 W = 1E-006
RD 10 1 0.0003964
RS 30 3 0.001
RG 20 2 13.18
CGS 2 3 8.007E-009
EGD 12 30 2 1 1
VFB 14 30 0
FFB 2 1 VFB 1
CGD 13 14 3.8E-009
R1 13 30 1
D1 13 12 DLIM
DDG 14 15 DCGD
R2 12 15 1
D2 30 15 DLIM
DSD 10 3 DSUB
.MODEL PMOS PMOS LEVEL = 3 U0 = 400 VMAX = 1E+006 ETA = 0.001
+ TOX = 6E-008 NSUB = 1E+016 KP = 763.4 KAPPA = 19.32 VTO = -1.08
.MODEL DCGD D CJO = 1.7E-009 VJ = 0.8 M = 0.6
.MODEL DSUB D IS = 2.712E-008 N = 1.174 RS = 0.0001033 BV = 25.5 CJO = 3E-009 VJ = 0.8 M = 0.6 TT = 1.2E-008
.MODEL DLIM D IS = 0.0001
.ENDS
*Diodes DMP2003UPS Spice Model v1.0M Last Revised 2017/10/13