Other Parts Discussed in Thread: TLV3201
Hi I have read the datasheet of TLV3201-Q1,
There has the curve of Output Voltage vs Output Current with full range temperature of 2.7V and 5.5V
but we are using 5V as the input voltage with tolerance ±1%,
so can TI offer the curve of Output Voltage vs Output Current with full range temperature of 5V±1%?
or the calculate between Vout with Temperature and Current
We are using as frequency oscillator, so the vout voltage will effect the RC time constant
Thanks for apply.