This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA190: Output ringing issue

Part Number: INA190

Dear Technical Support Team,

I have questions about INA190A2.

(question 1)
A ringing waveform has been confirmed for about 1.5 mS from the saturation of the output voltage to the stability.
Would you please tell me if there is a way to shorten it or eliminate ringing?

When the current flowing through the resistor 40Ω changes from 5mA to 0mA
A ringing waveform is observed at the output voltage.

(Question 2)
Even when the ENABLE signal is switched from OFF to ON, the ringing waveform is between about 150uS.
It will happen. Please let me know if you have any countermeasures for this as well.

■Configuration

Shunt resister 40Ω

REF is driven by 2V buffer AMP.

VS= 5V

Best Regards,

ttd