Part Number: INA301
Hello,
My Customer is considering the INA301A3. They want to configure current limiting circuits using analog or ALERT outputs.
Is there any example circuit that can be used as a reference?
To explain a little more what they want to achieve,
they monitor the current of 0.5A, 1A, 2A, 3A (default is 2A) and limit the current,
except that there is an inrush current of 10A when the power is turned on. They want to pass this inrush current.
After this inrush current, there is a requirement to enable the current limiting circuit 200ms later.
Best regards,
DDdoor